2024-07-05 07:19 AM
Hi, This is the first time im working with SMBUS peripheral and want to implement this for a project.
I have gone through AN4502 document for SMBUS but im having hard time understanding stack of SMBUS module.
why do we need stack for communication for just one SMBUS peripheral from STM32H7 board. whats the difference between SMBUS_StackHandleTypeDef & SMBUS_HandleTypeDef and whats use of this.
i have read the 6.1 Host side point from the same document and initialised things as mentioned in it.
MX_GPIO_Init();
MX_SMBus_PMBus_Stack_Init();
MX_I2C1_SMBUS_Init();
STACK_SMBUS_Init(&hsmbus1);
STACK_SMBUS_GetBuffer()
MX_SMBus_PMBus_Stack_Init();
STACK_SMBUS_HostCommand(&hsmbus1, 0x17, 10, 0x17);
but HAL_SMBUS_IsDeviceReady fnction returning HAL_ERROR in response.
can someone guide me in a right direction for this
2024-07-08 03:38 AM
Hello @_kalpesh
why do we need stack for communication for just one SMBUS peripheral?
SMBus is more than just I2C, it has additional features and requirements. The stack handles these additional features, ensuring reliable and correct communication. Using the stack simplifies your code and reduces the risk of errors.
Difference Between SMBUS_HandleTypeDef and SMBUS_StackHandleTypeDef:
To initialize and use the SMBus peripheral on your board: Initialize GPIOs, Initialize SMBus Peripheral, Initialize SMBus Stack finally Use the stack functions to perform SMBus communication.
Example of how to use the SMBus peripheral and stack:
#include "main.h"
#include "stm32h7xx_hal.h"
#include "smbus.h"
#include "smbus_stack.h"
// Global variables
SMBUS_HandleTypeDef hsmbus1;
SMBUS_StackHandleTypeDef hsmbus_stack;
// Function prototypes
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_I2C1_SMBUS_Init(void);
static void MX_SMBus_PMBus_Stack_Init(void);
int main(void)
{
// Initialize the HAL Library
HAL_Init();
// Configure the system clock
SystemClock_Config();
// Initialize all configured peripherals
MX_GPIO_Init();
MX_I2C1_SMBUS_Init();
MX_SMBus_PMBus_Stack_Init();
// Initialize the SMBus stack
STACK_SMBUS_Init(&hsmbus_stack);
// Example: Check if a device is ready
if (HAL_SMBUS_IsDeviceReady(&hsmbus1, 0x17 << 1, 10, HAL_MAX_DELAY) != HAL_OK)
{
// Handle error
Error_Handler();
}
// Example: Send a command
uint8_t command = 0x17;
uint8_t data = 0x10;
if (STACK_SMBUS_HostCommand(&hsmbus_stack, command, 1, &data) != STACK_OK)
{
// Handle error
Error_Handler();
}
// Main loop
while (1)
{
// Your application code
}
}
static void MX_GPIO_Init(void)
{
// Initialize GPIOs for SMBus
// This is typically done in the CubeMX-generated code
}
static void MX_I2C1_SMBUS_Init(void)
{
// Initialize the SMBus peripheral
hsmbus1.Instance = I2C1;
hsmbus1.Init.Timing = 0x00707CBB;
hsmbus1.Init.OwnAddress1 = 0;
hsmbus1.Init.AddressingMode = SMBUS_ADDRESSINGMODE_7BIT;
hsmbus1.Init.DualAddressMode = SMBUS_DUALADDRESS_DISABLE;
hsmbus1.Init.OwnAddress2 = 0;
hsmbus1.Init.OwnAddress2Masks = SMBUS_OA2_NOMASK;
hsmbus1.Init.GeneralCallMode = SMBUS_GENERALCALL_DISABLE;
hsmbus1.Init.NoStretchMode = SMBUS_NOSTRETCH_DISABLE;
hsmbus1.Init.PacketErrorCheckMode = SMBUS_PEC_ENABLE;
hsmbus1.Init.PeripheralMode = SMBUS_PERIPHERAL_MODE_SMBUS_HOST;
hsmbus1.Init.SMBusTimeout = 0x00008061;
if (HAL_SMBUS_Init(&hsmbus1) != HAL_OK)
{
// Initialization Error
Error_Handler();
}
}
static void MX_SMBus_PMBus_Stack_Init(void)
{
// Initialize the SMBus stack
hsmbus_stack.hi2c = &hsmbus1;
hsmbus_stack.State = SMBUS_STATE_READY;
hsmbus_stack.ErrorCode = SMBUS_ERROR_NONE;
hsmbus_stack.Timeout = HAL_MAX_DELAY;
}
void SystemClock_Config(void)
{
// Configure the system clock
// This is typically done in the CubeMX-generated code
}
void Error_Handler(void)
{
// Handle errors
while (1)
{
}
}
I hope my answer has helped you. When your question is answered please close this topic by marking as Best the reply that answered you, it will help others find that answer faster. Thanks for your contribution.