cancel
Showing results for 
Search instead for 
Did you mean: 

What to do with pin 9/T_JCLK of STLINK-V3MINIs 14pin connector

LMI2
Lead

I have STM32H750 100pin chip and STLINK-V3MINI. Pin 9 of mini 14 pin connector has no obvious place on the chip. There is already a JTCK/SWCLK signal between 6/14 and PA14/STM32H.

I am using AN4938 table 6 and UM2502 also table 6 to connect debug pins.

1 ACCEPTED SOLUTION

Accepted Solutions

On the typical ARM 10-pin, that's the KEY pin (missing), perhaps there is a JTAG variant of the cable/connector where this is the same as JTCK, or it provides a second clock for another chain/device.

I'd focus on SWCLK, SWDIO, SWO and NRST signals.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

2 REPLIES 2

On the typical ARM 10-pin, that's the KEY pin (missing), perhaps there is a JTAG variant of the cable/connector where this is the same as JTCK, or it provides a second clock for another chain/device.

I'd focus on SWCLK, SWDIO, SWO and NRST signals.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
LMI2
Lead

Yes, I have SWCLK, SWDIO, SWO and NRST signals handled. T_JCLK is just last "unhandled exception" in that connector.