cancel
Showing results for 
Search instead for 
Did you mean: 

What is the temperature range of the nucleo-u575zi-q evaluation board ?

Pintoo
Associate II

my goal is to use this board in [-40°C +85°C] climatic chamber.

Regards:)

Oliver

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Guru

The boards are meant for evaluation in a lab bench type environment. I don't think they're rated for a temperature range, but should work in the industrial temp range (-40 to +85) provided you keep humidity from condensing. Certainly the chip itself will work in this range. Might want to check the temp range of the crystal on the board if you're using it for a clock source.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

4 REPLIES 4
TDK
Guru

The boards are meant for evaluation in a lab bench type environment. I don't think they're rated for a temperature range, but should work in the industrial temp range (-40 to +85) provided you keep humidity from condensing. Certainly the chip itself will work in this range. Might want to check the temp range of the crystal on the board if you're using it for a clock source.

If you feel a post has answered your question, please click "Accept as Solution".
Pintoo
Associate II

According your answer, to check the component's temperature, where can I find the Bill Of Materials for the nucleo-u575zi-q evaluation board ?

TDK
Guru

If you go to the product page, you can find the design files, including the BOM, under "CAD Resources":

https://www.st.com/en/evaluation-tools/nucleo-u575zi-q.html#cad-resources

https://www.st.com/resource/en/bill_of_materials/mb1549_bom.zip

If you feel a post has answered your question, please click "Accept as Solution".
Pintoo
Associate II

Thank you TDK, I'm going to check the BOM to retrieve the operationnal temperature of the evaluation board Nucleo 144