2022-09-10 10:18 AM
I'm looking for connectors to populate CN11 and CN12 on the board, but all extended 2.54mm female connector I cound find have 11mm legs, those used by ST is only about 8.4mm.
If they are not the same length, I won't be able to plug the board on other base boards because the logger pins are in the way.
Is anyone knows the exact model of the original connector and where I cound purchase them?
2022-09-10 10:52 AM
PF254217D1531
All parts number you can find here:
https://www.st.com/en/evaluation-tools/nucleo-f767zi.html#cad-resources
Bill of Materials (BOM).
2022-09-10 11:14 AM
Zio is the arduino with double row headers. They are populated. Maybe to be precise, here the MORPHO connectors which are at the edge of the pcb, and unpopulated is the question related to?
2022-09-10 09:24 PM
Thanks for the information, I got the bom.
However, PF254217D1531 seems not available on digikey/mouser, is there any other source?
2022-09-10 09:25 PM
Yes, I want populate CN11 and CN12 which are "MORPHO" connectors, but I need to know the model of connectors used for "ST Zio" since I have to keep them the same hight and size