2020-12-30 05:12 PM
Hello,
I have recently bought the STEVAL-IDB008V1M with hopes of possibly integrating it into a product but I have run into a problem regarding the programming of the BlueNRG2-M2SA. When I connect the STLINK/V2 and run the ST LINK Utility it recognizes the BLUENRG2 device connected to it. The problem is, that when I try and debug it using something like TrueStudio the program is not able to download to the device. Also if I try Keil uVision, it says that the it cannot access device memory, this is after making sure that ST-LINKV2 and SWD were being used in the configuration. Using the BlueNRG Navigator I am able to install the example projects just fine through the USB. I am not sure why there is this issue when trying to use the STLINK/V2, any assistance will be appreciated.
Thanks,
Steven
2021-06-09 11:28 AM
I've got the some issue. Did you find a way to fix this?
Kind regards
2023-01-20 10:57 AM
Hi guys, same for me. Can't connect to the microcontroller using ST-link or keil :-(. USB bootloadr stay works.
Any help ?