2023-10-23 03:40 AM
Hi.
After firmware upgrade for st-link v2, windows computer recognized the st-link as universal serial bus instead of virtual com port. whenever i try to program to MCU, there is error like a "No target device found".
How can I solve it?
Below image is the device manager to be recognized as Universal serial bus. there is no PORT.
Thank advance.
BR
2023-10-26 02:51 AM
Has this ST-LINK successful connected with any MCU ?
The connectivity and functionality of this MCU looks to be non-functional. Can you connect via the System Loader with BOOT0 High? Say, getting the UART protocol to respond to interaction? Has the device been set into a read protect mode? Disabling th SWD?
2023-10-26 02:59 AM
I wired boot0 with gnd. It didn’t connect with mcu. Not read protection mode.
i flashed successfully this board before firmware upgrade for st-link v2. After this I can’t