cancel
Showing results for 
Search instead for 
Did you mean: 

STM32l412 Nucleo-32 Dev Board has shorted pins?

JReic.2
Associate

The following pins appear to be shorted on the STM32L412 Nucleo-32 Dev Board :

A4 (PA5) shorted to D4 (PB7)

and

A5 (PA6) shorted to D5 (PB6)

Is it possible someone can verify, I have checked four Nucleo-32 boards and all show the shorted pins. The Nucleo board also does show this shorted behavior when powered up in the system.

1 REPLY 1
JReic.2
Associate

OK, never mind, I downloaded the gerbers and found that there are 0ohm resistors connecting these pins. I am sure it is documented somewhere. Seems kinda odd.