cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L053 DISCOVERY PROBLEM

RGudo.1
Associate II

0693W000006FY9fQAG.pngHello,

I get this file in my board. What is the problem?

Updated all drivers, tried setting BOOT0 to high and then updated them but still nothing, any ideas?

P.S.

I tried to run one code was working fine. When tried to load other then this happend.

5 REPLIES 5

Hello

In STLink settings, change the reset options. Try "connect under reset" and / or use "hardware reset".

RGudo.1
Associate II

Just do what you tell me:

0693W000006FYG7QAO.pngBut get this error:

0693W000006FYGCQA4.png 

0693W000006FYGHQA4.png

RGudo.1
Associate II

Hello,

No man still error. I think the problem is somewhere else. I tried under reset, pre-reset, normal. Still errors.

But I can connect to stm32 ST-LINK UTILITY0693W000006FYXrQAO.png 

But in KEIL program can't connect

Select a slower connection speed​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..