2025-04-04 8:24 AM - last edited on 2025-04-04 10:53 AM by mƎALLEm
Hi everyone,
I’m working with the STM32H747I-DISCO board and its onboard QSPI flash (Micron MT25QL512ABB). I’m encountering a frustrating issue:
Problem:
Writes to even addresses (e.g., 0x90000000, 0x90000002) work perfectly.
Writes to odd addresses (e.g., 0x90000001, 0x90000003) either fail silently or corrupt data.
What I’ve tried:
Configured QSPI in 1-line and 4-line modes (with/without Memory-Mapped Mode).
Ensured sector erasure (4KB) before writing.
Used both PAGE PROGRAM (0x02) and QUAD PAGE PROGRAM (0x32) commands.
Verified signals with an oscilloscope (no obvious timing issues).
Questions:
Is this a hardware limitation of the QSPI flash or the STM32 controller?
What’s the correct configuration to write single bytes to odd addresses?
Should I force standard SPI (1-line) mode instead of Quad I/O?
/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file : main.c
* @brief : Main program body
******************************************************************************
* @attention
*
* Copyright (c) 2025 STMicroelectronics.
* All rights reserved.
*
* This software is licensed under terms that can be found in the LICENSE file
* in the root directory of this software component.
* If no LICENSE file comes with this software, it is provided AS-IS.
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "quadspi.h"
#include "gpio.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
#define SECTORS_COUNT 100
uint8_t writebuf[] = "Che bello ndar da Peepeee!!!";
uint8_t ReadBuf[100];
#ifndef HSEM_ID_0
#define HSEM_ID_0 (0U) /* HW semaphore 0*/
#endif
void TEST_QSPI();
void QSPI_Write_Byte(uint32_t address, uint8_t data);
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
/* USER CODE BEGIN PV */
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
/* USER CODE BEGIN PFP */
void Write_Byte_QSPI();
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
#include <string.h>
//#define SECTORS_COUNT 100
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* USER CODE BEGIN Boot_Mode_Sequence_0 */
// int32_t timeout;
/* USER CODE END Boot_Mode_Sequence_0 */
/* Enable I-Cache---------------------------------------------------------*/
SCB_EnableICache();
/* Enable D-Cache---------------------------------------------------------*/
SCB_EnableDCache();
/* USER CODE BEGIN Boot_Mode_Sequence_1 */
/* Wait until CPU2 boots and enters in stop mode or timeout*/
//timeout = 0xFFFF;
//while((__HAL_RCC_GET_FLAG(RCC_FLAG_D2CKRDY) != RESET) && (timeout-- > 0));
//if ( timeout < 0 )
//{
//Error_Handler();
// }
/* USER CODE END Boot_Mode_Sequence_1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN Boot_Mode_Sequence_2 */
/* When system initialization is finished, Cortex-M7 will release Cortex-M4 by means of
HSEM notification */
/*HW semaphore Clock enable*/
__HAL_RCC_HSEM_CLK_ENABLE();
/*Take HSEM */
//HAL_HSEM_FastTake(HSEM_ID_0);
/*Release HSEM in order to notify the CPU2(CM4)*/
//HAL_HSEM_Release(HSEM_ID_0,0);
/* wait until CPU2 wakes up from stop mode */
//timeout = 0xFFFF;
//while((__HAL_RCC_GET_FLAG(RCC_FLAG_D2CKRDY) == RESET) && (timeout-- > 0));
//if ( timeout < 0 )
//{
//Error_Handler();
//}
/* USER CODE END Boot_Mode_Sequence_2 */
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_QUADSPI_Init();
/* USER CODE BEGIN 2 */
//TEST_QSPI();
Write_Byte_QSPI();
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Supply configuration update enable
*/
HAL_PWREx_ConfigSupply(PWR_DIRECT_SMPS_SUPPLY);
/** Configure the main internal regulator output voltage
*/
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.HSIState = RCC_HSI_DIV1;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 2;
RCC_OscInitStruct.PLL.PLLN = 32;
RCC_OscInitStruct.PLL.PLLP = 2;
RCC_OscInitStruct.PLL.PLLQ = 2;
RCC_OscInitStruct.PLL.PLLR = 2;
RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_3;
RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;
RCC_OscInitStruct.PLL.PLLFRACN = 0;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
|RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2;
RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2;
RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
{
Error_Handler();
}
HAL_RCC_MCOConfig(RCC_MCO1, RCC_MCO1SOURCE_HSI, RCC_MCODIV_1);
}
/* USER CODE BEGIN 4 */
void TEST_QSPI()
{
uint8_t buffer_test[MEMORY_SECTOR_SIZE];
uint32_t var = 0;
CSP_QUADSPI_Init();
for (var = 0; var < MEMORY_SECTOR_SIZE; var++) {
buffer_test[var] = (var & 0xFF);
}
for (var = 0; var < SECTORS_COUNT; var++) {
if (CSP_QSPI_EraseSector(var * MEMORY_SECTOR_SIZE,
(var + 1) * MEMORY_SECTOR_SIZE - 1) != HAL_OK) {
while (1)
; //breakpoint - error detected
}
if (CSP_QSPI_WriteMemory(buffer_test, var * MEMORY_SECTOR_SIZE, sizeof(buffer_test)) != HAL_OK) {
while (1)
; //breakpoint - error detected
}
}
if (CSP_QSPI_EnableMemoryMappedMode() != HAL_OK) {
while (1)
; //breakpoint - error detected
}
for (var = 0; var < SECTORS_COUNT; var++) {
if (memcmp(buffer_test,
(uint8_t*) (0x90000000 + var * MEMORY_SECTOR_SIZE),
MEMORY_SECTOR_SIZE) != HAL_OK) {
while (1)
; //breakpoint - error detected - otherwise QSPI works properly
}
}
}
void Write_Byte_QSPI() {
int i = 0;
if(CSP_QUADSPI_Init() != HAL_OK)
{
Error_Handler();
}
if(CSP_QSPI_Erase_Chip() !=HAL_OK)
{
Error_Handler();
}
if(CSP_QSPI_WriteMemory(writebuf,0, sizeof(writebuf))!=HAL_OK)
{
i = 1;
}
if(i ==1)
{
HAL_GPIO_WritePin(GPIOI, GPIO_PIN_13, GPIO_PIN_SET);
}
}
/* USER CODE END 4 */
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
__disable_irq();
while (1)
{
}
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* file: pointer to the source file name
* line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
Additional Context:
Board: STM32H747I-DISCO
Flash: Micron MT25QL512ABB (512Mbit, QSPI/OPI)
Toolchain: STM32CubeIDE 1.11.0 / HAL 1.11.0
Solved! Go to Solution.
2025-04-07 6:06 AM
Hi Guys,
I used our suggestion and I want to share my results............
I found this tutorial https://github.com/gokmez/STM32H7-Bootloader/tree/master but the mt25tl01g.h file is wrong....So I change it with https://github.com/controllerstech/STM32/tree/master/QSPI/MT25TLxxx and it works!!!!
Thank you again
2025-04-04 9:31 AM
I think the External Loader is looking at a pair of memories, or dual die TL part.
The banks alternate odd/even bytes
In single part mode you'll only program one part, the even one
2025-04-04 10:36 AM - edited 2025-04-04 10:38 AM
They use the DUAL FLASH mode, so a pair of MT25QL512 or dual die MT25TL01G, allows for an 8-bit interface, higher bandwidth, achieved by alternating bytes between both, ie sends one command and you write a page of 512 bytes, rather than the 256 bytes for a single memory. Same for reads of status registers, reading a pair of bytes and waiting when either is BUSY or JEDEC READ ID, where you'd now read 6-bytes instead of 3
The External Loader for the H747I-DISCO presumes the paired devices. You could access a singular device loader, then it would see the data as you read it. There should be a workable loader on my github repo to access just the one device.
PB2,PG6,PD11,PF9,PF7,PF6 (CUSTOM19) H747I-DISCO LOW BANK
https://github.com/cturvey/stm32extldr/tree/main/h7_mt25ql512a
2025-04-07 6:06 AM
Hi Guys,
I used our suggestion and I want to share my results............
I found this tutorial https://github.com/gokmez/STM32H7-Bootloader/tree/master but the mt25tl01g.h file is wrong....So I change it with https://github.com/controllerstech/STM32/tree/master/QSPI/MT25TLxxx and it works!!!!
Thank you again