2022-01-15 7:40 AM
Hello All,
I have a certain STM32H7 that I can't erase sector 0 using STM32CubeProgrammer.
I think it is because PROT_AREA_START1 and PROT_AREA_END1 are not correct. I am trying to get back to default values of
PROT_AREA_START1 =0xFF (0x0800ff00)
PROT_AREA_END1 = 0x00 (0x080000ff) to disable the protection.
However I cant Actually change the option bytes through the programmer. I get:
an error: "Expected Value for option byteP: "PROT_AREA_START!: 0xFF, fount 0x00"
RDP is level 0 (AA)
I am using ST-link. Thanks for any help,
Trevor
2022-01-17 5:37 AM
Hello Trevor,
could you please share your STLink configuration?
Did you try to disconnect/connect your board?
The Security bit is disabled?
nWRPx = 1?
BR
Chloé
2022-01-17 9:30 AM
2024-03-10 11:49 PM
Hi,
I have the same problem, does someone have a solution?
Y.H
2025-01-23 2:34 AM - edited 2025-01-23 2:37 AM
Hi,
I am Facing Problem please suggest Some solution
i attached Batch Script running for changing option bytes and stm32cubeprogrammer.
Regards,
Prakash
2025-02-27 11:39 PM - edited 2025-02-27 11:39 PM
still No response
Regards,
Raja