2023-08-15 8:36 AM
Hi,
My nucleo stm32g0b1re board is failed connect after option byte Boot0 checked in Flash Security.
I've tried many ways to connect board/ease modified SBSFU on the flash but no luck. could someone help me to recover board?
TIA
2023-08-15 6:40 PM
Hello @Tarun ,
If you are unable to connect to your Nucleo STM32G0B1RE board after enabling the Boot0 option byte in Flash Security, it is likely that the board is stuck in bootloader mode. To resolve this issue, you can try the following steps:
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-08-16 2:48 AM
Hi Foued,
I shorted pin 7 and 8 in the image but still same error seen on the Cubeprogrammer. Is am I missing anything?
TIA
2023-08-26 1:08 AM
Sorry it didn't helps. I have to replace my dev kit.