cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G071RBT6(Reason : (4)No device found on target.)

Bryan_KIM
Associate II

Hello,

I have the following problem when using the Nucleo board.

I do not have a mini-usb.

So I use to ST-LINK.

However, the following warning message is displayed.

Please tell me the solution.

Thank you for reading.

※ I use to STM32CubeIED.

0693W000003BUZzQAO.png0693W000003BUXeQAO.jpg

6 REPLIES 6
prain
Senior III

check that gnd, swdio, swclk lines are correctly shared between stlink and MCU. use a multimeter to check​

KnarfB
Principal III

Check you power supply. I would suggest connecting to VIN not VDD directly.

Thank you for the answer.

I linked it like the datasheet below.

but it isn't operation.

0693W000003BZ5tQAG.png

Thank you for the answer.

I linked it like the datasheet below.

but it isn't operation.

CN11

1 - VCC

2 - SWCLK

3 - GND

4 - SWDIO

5 - RESET

0693W000003BZ6IQAW.png

Can't in-bound SWD connection via that header, not how it works.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

That's for OUT-BOUND connectivity.

Review the schematic, understand the circuit..

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..