cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G071R8T6 GPIO - input issue on PA4

MPF
Associate II

Hi,

We have a custom board with a STM32G071R8T6TR, PA4 is configured as input but it does not work.

All other inputs on the boards are working correct but PA4 is a problem.

If we configure PA4 as an output it works fine, we toggle hi/lo, we have checked IDR for PA4 and the IDR does not change which is a problem, it does that when we toggle PA5 and PA6 hi/lo the IDR for PA5 and PA6 change.

If PA4 is configured as input and we change input hi/lo there is no change in IDR either.

We have cheked MODER is correct.

What do we miss here or could this be a defect STM32 MCU ?

Kind regards

Morten

 

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
MPF
Associate II

Hi,

We found the problem, its a problem with the MCU, in other similar products we don't see the issue.

We will replace the MCU.

BR
Morten

View solution in original post

11 REPLIES 11
waclawek.jan
Super User

Sounds much like hardware damage.

Do you have a second board, perhaps a Nucleo?

JW

AScha.3
Super User

Hi,

did you check real connection to pin exists ?

Try re-solder pin, maybe has bad solder joint.

(Funny is: if you check with DMM or scope, pressing on the pin is enough, to see: is ok.

But is not - as soon, as you no more press on the pin ! )

If you feel a post has answered your question, please click "Accept as Solution".

Hi Jan,

I think we should buy one, tested code and verified registers on STM32F411 nucleo, it works fine.

BR
Morten

Hi AScha.3,

Please read my description, IDR does not change when we configure as output and toggle PA4 hi/lo, IDR does change when we do that on other pins PA5, PA6.

Kind regards

Morten

 

waclawek.jan
Super User

Just to be sure:

> If we configure PA4 as an output it works fine,

this means, that you set PA4 as GPIO Output toggled it, and measured the output using logic analyzer/oscilloscope, correct?

JW

Hi JAn,

Yes this is correct.
So when PA4 is configured to output  and is set to 0 we read IDR as 0 - this is ok.

When we set PA4 to 1 we still read IDR as 0 even though we see 1 on the oscilloscope. 

If we do the above on other pins like PA5 and PA6 this works perfect.

Kind regards

Morten

 

waclawek.jan
Super User

Assuming this is a minimal code doing nothing else but toggling that pin (i.e. no analog features setup), all clues point to damaged mcu, then.

Note, that PA4 and PA5 are not 5-volt tolerant.

JW

Hi Jan,

We went back to basics and we are running from a very basic program using no other features. :)

Yes the pins work at 3.3V.

MPF

Did you check GPIO_LCKR?