cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F407VET6 and a 7" display

Ethan_Daugherty
Associate II

I am trying to design a system that use the STM32F407VET6 and a 7 inch LCD display that use LVDS. The screen is 1024x600 pixel resolution and can use 6-bit or 8-bit LVDS interface. The screen also uses a HX8282 LCD controller. I was wondering if I need a LVDS transmitter like the SN75LVDS84 to interact with the microcontroller. I want to be able to display a UI on the screen. Is there any example code for doing this or projects that I might be able to look at to help aid in my design process?

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5

No, you're wasting your time.

The F407 likely doesn't have sufficient memory for a frame buffers, and isn't designed to drive a TFT display.

The STM32F429 or F469 with an SDRAM off the side might be a starting point, or frankly one of the newer designs.

Or a LCD board with a controller and video RAM you can interface via the FSMC of the F407

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

If I changed to the F469 would it have the same pin layout as the F407 or is it completely different? How much SDRAM would be the minimum needed?

100-pin device might be a tad difficult.

Smallest SDRAM you'd likely be able to source is 64Mbit (8MB). High resolution video, probably want 32-bit wide. DSI would reduce pin count to a suitable display.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

If my 7" LCD screen has a LCD controller integrated into it would I need to have an STM32 that would be able to drive a TFT screen or would the controller in the screen be able to do it? I trying to figure out the design possibilities before I make a decision on it. Would it be the easiest option to switch the microcontroller to the STM32F469 or the F429 and use SDRAM with it?

https://www.buydisplay.com/download/ic/LT7683.pdf

Several panels are available from BuyDisplay using this controller, and it's on-board 128Mb (16MB) of display memory

https://www.buydisplay.com/7-inch-1024x600-ips-tft-touch-display-module-with-i2c-spi-for-arduino

https://www.buydisplay.com/download/ic/RA8876.pdf

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..