cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F407 First Programming Failed

ÀTorr.1
Associate

Hello Community!

I have a project where I was using a STM32F407 MCU from a minimal ready-to-run system with USB, programming connection and pin headers to access every MCU pin. While using this hardware, the project can be loaded and executed on the MCU.

However, to improve the hardware solution I integrated all these features in my own PCB and buy the MCU. The problem is that when connecting it for the very first time to STM32CubeProgrammer the system does not find the target at all.

I have checked the following things on the MCU pins:

  • Power supply 3.3V is OK
  • MCU current consumption is in the order of uA, lower than the specified by STM in the hardest Energy Saving mode.
  • Continuity from MCU pins and Progrrammer connector is OK
  • Clock signal from ST-Link Device is properly reaching the MCU.
  • Boot pins are properly managed by the programmer

The error raised by the STM32CubeProgrammer is the same as if there were no MCU connected: NO STM TARGET FOUND!

I bought a batch of 10 MCUs and the error is the same on the 4 different MCUs that I checked, also on PCBs from different manufacturers.

So far, I want to ask to the community the following:

  1. Is there any special status in which the MCUs are sent from factory that must be change before the very first programming? If yes, which is the procedure?
  2. Can you suggest me other points to check to validate the correct mounting and that the connection between ST-Link and MCU is OK?

Thank you all in advance for your help, I will appretiate your answers a lot.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Hello

>>?Is there any special status in which the MCUs are sent from factory that must be change before the very first programming? If yes, which is the procedure?

There is no any special treatment before first start.

>>Can you suggest me other points to check

AN4488 from ST has a lot of information about HW considerations and checks

>>Clock signal from ST-Link Device is properly reaching the MCU.

You probably mean the SWCLocK signal. But you didn't mention SWDIO pin and GND that are required to connect properly the STLink with board.

View solution in original post

2 REPLIES 2

Hello

>>?Is there any special status in which the MCUs are sent from factory that must be change before the very first programming? If yes, which is the procedure?

There is no any special treatment before first start.

>>Can you suggest me other points to check

AN4488 from ST has a lot of information about HW considerations and checks

>>Clock signal from ST-Link Device is properly reaching the MCU.

You probably mean the SWCLocK signal. But you didn't mention SWDIO pin and GND that are required to connect properly the STLink with board.

Dear Vangelis,

Thank you very much for your comments.

Finally, thanks to the AN4488 I have been able to find that there was a pin mismatching on BYPASS_REG. Now it seems to works properly.