2023-08-30 09:44 AM - edited 2023-08-30 09:45 AM
Hi Guys,
- I am using an STLINK-V3MINIE with the latest firmware as shipped with STM32CubeIDE v1.13.1.
- I am using MacOS 11.7.9 (Big Sur).
- I can successfully program my target using this STLINK-V3MINIE with STM23CubeProgrammer, but never with the IDE. Every time I attempt to debug my target, the session terminates because the programmer throws a flash programming error.
- I can successfully program and debug my target using the STLINK on a NUCLEO board.
- The STLINK-V3MINIE and NUCLEO board SWD leads are roughly the same length.
What can I try to get my STLINK-V3MINIE working? Any help is appreciated!
2023-08-30 11:09 AM
> Every time I attempt to debug my target, the session terminates because the programmer throws a flash programming error.
Show the error.
Does "Run" work?