2026-06-02 6:14 AM
hi ,
is there a easiest way to shift the STLINK v3 from ISOL to normal , during debugging it is ok with ISOL as the device has power.
but if i want to just use as a programmer without external power, then i have to remove the isol board and put back the jumpers .
is there a easiest way
2026-06-02 7:01 AM
Just to be clear, you're talking about the STLINK-V3SET with B-STLINK-ISOL adapter board - yes ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.