cancel
Showing results for 
Search instead for 
Did you mean: 

ST-Link V3 Not Detected, Only a Faint Red LED - Is it Dead?

biopunk101
Associate II

Hi everyone, I'm having an issue with a brand new ST-Link V3 and would appreciate a quick sanity check before I return it.

Here's the situation:

* The device is not detected by my PC at all (it does not appear in Device Manager).

* I have already confirmed my USB-C data cable is working correctly.

* The red power LED on the ST-Link is extremely faint and dim.

* I also tested it on a second computer, and the result was exactly the same.

Since the LED is so dim and it fails on multiple PCs, I'm confident this is a hardware fault (DOA). Has anyone seen this specific issue before? I've attached a photo of the dim LED.

 

Thanks for any input!

 

IMG_5514 大.jpeg

10 REPLIES 10
CeDeROM
Associate III

Thanks @S C for the confirmation :)

Are there any plans / dates for full speed mode to be implemented in STLINK-V3? :)

This firmware is not Open-Source right?