cancel
Showing results for 
Search instead for 
Did you mean: 

st link/v2,no target connected

vinothraj
Associate II
Posted on November 30, 2012 at 15:28

hi,

i have stm32f407vgt6 controller ic and stlink/v2.

the controller is fitted in our own board.i tried to program the controller.but it failed.it show like ''no target is connected''.i did the following connection.

Stlink pins                         stm pins

9      (SWCLK)              ----->           76(PA14)

20 (GND)     ------>         74(GND)

7   (SWDIO)   ----->    72 (PA13)

15 (NRST)    ----> 14 (NRST)

13 (SWO)  ------> 89 (PB3)

BUT i got wrong.can any one suggest any idea?

#st-link/v2 #no-target-connected
1 REPLY 1
Posted on November 30, 2012 at 16:40

Sounds like it's not powered and functional.

Check supply VSS/VDD (A and D)  and VCAP pins.

Bring up chip with BOOT0 High, check if you can get USART1 or USART3 to respond to 0x7F at 9600 8E1
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..