2025-01-10 07:29 AM
Hello All,
I am using stm32f405rgt6 with ST-Link v2.
I built the minimum circuit searching from internet.
When i am trying to upload the code, it gives me following.
Can any body help me on this.
STMicroelectronics ST-LINK GDB server. Version 7.9.0
Copyright (c) 2024, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61235
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Target no device found
Error in initializing ST-LINK device.
Reason: No device found on target.
and below-
Error in final launch sequence:
Failed to execute MI command:
target remote localhost:61238
Error message from debugger back end:
localhost:61238: Connection timed out.
Failed to execute MI command:
target remote localhost:61238
Error message from debugger back end:
localhost:61238: Connection timed out.
localhost:61238: Connection timed out.
Also if any body can suggest some good blog or tutorial for stm32f405rgt6 with custom board would be well appreciated.