cancel
Showing results for 
Search instead for 
Did you mean: 

SMPS power Regulator is not being set in STM32U575.

nilesh-dryad
Associate III

I am trying to set up SMPS power Regulator for low power operation. I am using Nucleo-U575ZI-Q board. I set the bit in CR3 register but bit in SVMSR is not being set.

Do anyone have idea what can be wrong? Is there something that I am missing?

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10

No, U575 SMPS is working at both 1.8V and 3.3V

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.