cancel
Showing results for 
Search instead for 
Did you mean: 

Setting Device Protection via ST-LINK

infoinfo990
Associate
Posted on July 29, 2011 at 13:48

I would like to set protections on a STM32F107 using the STVP Programming toolkit with the ST-LINK.

There are no examples of doing this in the toolkit. The GetProtectionList function for the devices lists no protections.

The GUI project edit dialogue do not have a protection section although the help says it should.

#st-link-stvp-programming-toolkit
0 REPLIES 0