cancel
Showing results for 
Search instead for 
Did you mean: 

Reference Design Availability for STM32WLE5JC (Schematics, PCB, RF Layout, Stack-up)

Vimukthi-Wathudura
Associate

Hi all,

I am currently working on the design of a custom LoRa/LoRaWAN-based IoT node using the STM32WLE5JCI6TR (bare MCU, not a module), and I am looking for a complete and reliable hardware reference design to follow.

So far, I have identified the following:

  • NUCLEO-WL55JC reference design files (schematics and PCB) from ST, which appear to be the closest official reference (even though it is based on WL55 dual-core variant)

  • Wio-E5 Dev Board from Seeed Studio, which is based on a module and does not expose the RF design details

While these are helpful, I am specifically looking for:

  1. A reference design based directly on STM32WLE5JC (or very close variant)

  2. Complete design files including:

    • Full schematics

    • PCB layout files

    • RF matching network implementation

    • Antenna routing

    • PCB stack-up / layer information

Since RF design (matching, impedance control, grounding, etc.) is quite sensitive, having a proven reference is critical.

Additionally, I would like to know:

:backhand_index_pointing_right: Are there any open-source or freely available reference designs based on STM32WLE5JC that include full PCB and RF layout details?

Any guidance, shared designs, or recommendations would be greatly appreciated.

Thanks in advance!

1 ACCEPTED SOLUTION

Accepted Solutions
Imen.D
ST Employee

Hello @Vimukthi-Wathudura and Welcome to the Community,

Please refer to the following resources:

STM32WL5x-Ex wireless MCU lines - Wireless MCUs System-on-Chip Long-range communications

Data brief - STDES-WL5xxxxx - Reference designs for STM32WL5x and STM32WLEx microcontrollers

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

View solution in original post

1 REPLY 1
Imen.D
ST Employee

Hello @Vimukthi-Wathudura and Welcome to the Community,

Please refer to the following resources:

STM32WL5x-Ex wireless MCU lines - Wireless MCUs System-on-Chip Long-range communications

Data brief - STDES-WL5xxxxx - Reference designs for STM32WL5x and STM32WLEx microcontrollers

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen