2024-10-15 2:23 AM
Hi
I am currently controlling a Fluke serial device over RS232 from a laptop and python script. I simply send requests for information which is returned and logged in my laptop. I'm using a Startech RS232 to USB lead incorporating the Prolific - PL2303RA chipset.
This is a simple setup but obviously requires a laptop to function so I have moved to an STM32F7 board in an attempt to separate from the PC.
I'm writing the same command from the ST board as I was sending from Python, from UART to a Seeed RS232 adapter. Scoping signals at this point shows them to be ok, whilst not connected to any serial device, yellow being UART and blue, RS232.
However, once I connect to my Fluke device the signals are corrupted to the point if illegibility:
I have reproduced the behaviour using a second UART -> RS232 interface and also switched out the Fluke device for another one from a different manufacturer, but no change in behaviour.
The Seeed interface can be found at 103990363 Seeed Studio | Mouser United Kingdom and uses the MAX3232 chip, whilst the Mikroe one is at MIKROE-222 Mikroe | Mouser United Kingdom and uses the MAX232 chip. There is a slight difference with how they arrange the capacitors which has some affect on their behaviour.
I'd appreciate any input regarding overcoming this final step of connecting to a serial device as I have hit a wall. Happy to supply any further information that may help find a solution.
Many thanks
Ian
2024-10-15 2:36 AM
Do you have a good ground connection between your SMT32 board, adaptor, and the Fluke?
Please show a schematic.
Some good, clear photos may also help.
Any specifications for the "Fluke serial device" ?
2024-10-15 3:27 AM
Hi Andrew
Thanks for getting back so quickly, I am utilising UART5 as highlighted below and taking 5V and GDN to the Seeed board. Grounding is commoned up from the STM32 through the Seeed interface and into the serial leads, I believe it is sufficient. Any scoping has been done with connection to this ground.
I hope the image below is sufficient to show what I am doing, I'm using a serial splitter to scope the output of the RS232 interface.
The Fluke device is a 6102 micro bath, I have no definitive spec of it's internals unfortunately beyond a reply from their technical support saying they use roughly 2µF capacitors in relation to their MAX232 serial setup.
The Seeed chip uses 0.1µF, could this potentially be an issue?
Ian
2024-10-21 4:04 AM
Hi Andrew
Do you need any further information regarding my question, unfortunately I cannot get anymore useful info regarding the Fluke 6102. The other unit I have tried, which behaves in almost the same way is a WIKA CPC 2000, I am trying to get further tech specs on that.
Best regards
Ian
2024-10-21 4:23 AM
@IPrin.1 wrote:Grounding is commoned up from the STM32 through the Seeed interface and into the serial leads, I believe it is sufficient
So how does that differ from the working case with the laptop?
2024-10-23 12:28 AM
Hi
Apologies for not responding yesterday I was away from work.
The grounding is the same between both cases, all USB leads are grounded correctly, as is the RS232 - USB adapter in the working case. This is the same for the non-working case, grounding is continous through the leads, ST boards and serial leads.
Ian
2024-10-23 12:29 AM
I'm out of ideas, then.
2024-10-23 12:36 AM
No problem, thanks for looking into this. If I find a solution I will post it here.
Ian