2025-09-16 9:35 AM
I want to program a NUCLEOWB55RG board with another identical NUCLEOWB55RG.
The reason is the other NUCLEO board is placed on a PCB and is powered externally, so i cannot connect USB to it.
Do I just remove the JP1 jumper and connect the SWD pins (SWD, SWDIO, GND, VDD, NRST) between boards?
Solved! Go to Solution.
2025-09-16 10:25 AM - edited 2025-09-16 11:42 AM
Hello @fshaikh98
I advice you to use the JP5 of both boards for connections. You may also refer to this article with this article too.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-09-16 9:56 AM
Why is connecting USB a problem? If external power is connected, it'll use that instead of USB if you have the jumpers configured appropriately.
But yes, if you connect SWDIO/SWCLK/GND/SWD at the JP5 header, it should work. JP1 is a power header, doesn't seem relevant here.
2025-09-16 9:58 AM - edited 2025-09-16 9:59 AM
@TDK External power is 3.3V here, not 5V. I am afraid of the regulator's output affecting the 3.3V input
2025-09-16 10:25 AM - edited 2025-09-16 11:42 AM
Hello @fshaikh98
I advice you to use the JP5 of both boards for connections. You may also refer to this article with this article too.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.