2019-07-24 8:57 AM
I note that the STM32H750B-DK comes with an attached display. If required for evaluation / development, can a larger display be connected in its place? Something in the 8" to 10" range. Touch is not needed. If so, can you recommend any brands and/or model numbers that could be connected in place of the attached display? Additionally, can the attached display be easily removed?
Thank you,
Dennis
Student,
ME program,
Washington State University.
2019-07-24 10:50 AM
Board doesn't look to be designed to remove/replace the screen. I'm sure it could be removed with brute force, but not going to recommend that as a course of action. You'd need to be really sure you can find compatible displays.
For a detachable screen look at the STM32H747I-DISCO(DK) , it use DSI/MIPI (2 lanes) via a mictor like connector. Resolution likely to be constrained by bandwidth.
The DISC1 variant of board is cheaper, and doesn't ship with a screen.
Should take HDMI adapter board, would drive a monitor via HDMI/DVI. Need to work on drivers, to get a selection of resolutions.
For other displays you'd need to review specifications, and make an adapter board. Seem to encountered a couple of DSI-to-Panel IC's so potential options there.
The H743I-EVAL board exposes the parallel LCD signals to a header/ribbon cable, ST has a couple of displays.