NUCLEO-F767ZI unable to do a FullChipErase
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-03-29 1:33 AM
Hi,
i was playing with OptionBytes on my custom USB-Bootloader and... I end up in a bricked NUCLEO board... the CPU itself is still running (I can even update an application) but I cannot connect via ST-LINK and/or DfuSe anymore...
The error message is:
09:12:27 : Can not connect to target!
If you're trying to connect to an STM32W1xx device, please select Normal or HotPlug mode from Target->Settings menu.
If you're trying to connect to a low frequency application , please select a lower SWD Frequency mode from Target->Settings menu.
09:12:28 : No target connected
On the device folder:
DETAILS.TXT
------------------
Version: 0221
Build: Sep 18 2018 11:09:21
FAIL.TXT
------------
The interface firmware FAILED to reset/halt the target MCU
ST-Link utils is v4.3.0.0
ST-LinkUSB-Driver is v5.1.0.0
ST-Link CLI is v3.3.0.0
The option "connect under reset" & pressing the B2 (reset) button before doing a chip erare seems not to work... somewhere there is a note regarding SB111 (pad between NRST-RST) but in my case a 0 ohm resistor is already there.
Any ideas on how to unbrick my NUCLEO board ?
thanks,
Giampaolo
- Labels:
-
ST-Link
-
STM32F7 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-03-29 2:47 AM
Try connect under reset or USB DFU.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-03-29 2:55 AM
Hi Uwe...
I've already done this... and it did not work... I think I'm somehow in Level 2 protection:
Level 2 is an irreversible operation. When Level 2 is activated, the level of protection cannot be decreased to Level 0 or Level 1.
Giampaolo
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-03-29 3:04 AM
> Try connect under reset or USB DFU
Booting into system mode, and try a mass-erase there ?
Not sure if this is meant to be the same.
> I think I'm somehow in Level 2 protection:
>Level 2 is an irreversible operation. When Level 2 is activated, the level of protection cannot be decreased to Level 0 or Level 1.
Then you have bricked it probably ...
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-03-29 3:16 AM
uh...
I was convinced that full chip erase was always possible... but it seems that I was wrong... my bad.
Giampaolo
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-03-29 3:30 AM
There are hacks out there that that will turn Level 2 into level 1. Look at the CC (Computer Chaos ) Club conferences talks. In short, they turn on the chip and turn off at the right moment. But buying a new Nucleo is much less effort.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-03-29 3:55 AM
Hello Uwe...
.. I was also thinking at replacing the MCU... but since it costs $13 while the whole board is $20... it's a nonsense...
I've done a search for CCC and STM32 Level 2 but got nothing... do you have a link to the paper you are talking about ? I'm just curious....
tnx
Giampaolo
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-03-29 4:03 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-03-29 4:40 AM
amazing!
tnx Uwe...