cancel
Showing results for 
Search instead for 
Did you mean: 

no device found on target stm32f407g

vyıbjf67
Associate II

hi, i got this error on stm32cubeide. I've used my board 3 weeks ago. I can't neither start the program I loaded before nor load the new program. can see Stmicroelectronics STLink Virtual COM Port COM 5 on device manager. how to solve this problem?

This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
STTwo-32
ST Employee

Hello @vyıbjf67 and welcome to the ST Community :smiling_face_with_smiling_eyes:.

Please check that the jumpers are correct on your board, especially the one for the ST-LINK.Then, try to connect your board with STM32CubeProgrammer. In the ST-LINK configuration area, try the following configuration:

  • Serial number: Refresh to get your ST-LINK serial
  • Mode: Under reset
  • Reset mode: Core reset

Finally, try to connect your board.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

What should I do?

ST-LINK Utility is obsolete. You have to use the STM32CubeProgrammer.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

vyıbjf67
Associate II

How can I use CubeIde?

Which board are you using? The DISCO or NUCLEO? Something else?

Make sure the pair of ST-LINK jumpers are in place.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Discovery and jumpers are in place.