2023-08-25 5:55 AM
I didn't have a suitable microcontroller available and I have to use what is available, but the problem is that I have a lot of unused pins and I also work with Battery, so according to the documents, I decided to make the unused pins analog inputs.
But I have 2 questions:
1-Is the analog input the same as GPIO_ANALOG in the cube?
2- when it is set in this way, do we need to use external pullup/pulldown resistors?
Solved! Go to Solution.
2023-08-25 6:05 AM
1. Yes
2. No, you can leave them floating. The internal Schmitt triggers are disconnected in analog mode.
2023-08-25 6:05 AM
1. Yes
2. No, you can leave them floating. The internal Schmitt triggers are disconnected in analog mode.