Skip to main content
Dubey
Associate
Jan 19, 2021 11:35 AM UTC
Solved

MCU STM32F091VCT6 is in continuous reset mode.

I'm using STM32F091VCT6 controller. I'm tried to BOOT it. MCU does not stand by mode (either low power mode or continuous reset mode). I'm tried by increasing delay on VCC & POR by using 10uf cap of NRST pin also I'm tried weak pull down on BOOT0 pin(47K to 10K register value) also please suggest how I will check exact behave of controller ??

This topic has been closed for replies.
TDK
TDKBest answer
Jan 19, 2021 1:17 PM UTC

NRST should have a 0.1uF capacitor on it, nothing more. BOOT0 needs pulled down. If you do that, and apply power, the chip will start executing code.

You can always attach a debugger to see where the chip is at.

"If you feel a post has answered your question, please click ""Accept as Solution""."

2 replies

TDK
TDKBest answer
Jan 19, 2021 1:17 PM UTC

NRST should have a 0.1uF capacitor on it, nothing more. BOOT0 needs pulled down. If you do that, and apply power, the chip will start executing code.

You can always attach a debugger to see where the chip is at.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Dubey
DubeyAuthor
Associate
Jan 20, 2021 4:28 AM UTC

Thanks TDK.