2022-06-14 7:27 AM
Hi, I made a minimum CubeIDE project for a Nucleo-L4R5ZI. It clocks the RTC from LSE using the X2 quartz (NX3215SA-32.768kHz-EXS00A-MU00525) and outputs a 512Hz calibration signal on PC13. The output frequency is only ~492Hz which is a deviation of ~5%. I couldn't find any reasonable explanation. Any ideas?
Solved! Go to Solution.
2022-06-15 6:08 AM
By the way:
I just realized that you can output the LSE clock directly to MCO (PA8 on STM32L4R5ZI), so you can scope the decoupled LSE signal directly.
2022-06-19 11:14 PM
Hi,
I just tested 3 other Nucleo-L4R5ZI boards: They were all fine with the factory capacitors. It looks like only that one specimen I had on the table was faulty.