2017-12-14 9:57 AM
I see there some have problems (the board doesn't work well anymore) after separating the programmer part from the rest of the board. And I intend to use this tool to cut the bridges...
Solved! Go to Solution.
2017-12-14 10:06 AM
Load the Gerbers into a viewer?
http://www.st.com/resource/en/board_manufacturing_specification/nucleo_64pins_gerber.zip
2017-12-14 10:06 AM
Load the Gerbers into a viewer?
http://www.st.com/resource/en/board_manufacturing_specification/nucleo_64pins_gerber.zip
2017-12-14 11:20 AM
So two layers... thank you Clive! There may be several chances to have bridged traces on the bottom layer on a rough cut, and one for the top layer...
I recommend to make those PCB bridges wider and the traces with more space between them.
Or on the microcontroller board, 0 ohm resistors as a bridge for the signal traces, that can be un(de)-soldered to avoid short circuit after a separation.