cancel
Showing results for 
Search instead for 
Did you mean: 

Inconsistent package naming in Cube32MX - MCU Selector

Andreas Bolsch
Lead II

What's the difference between "LQFP32" and "LQFP 32 7x7x1.4mm"? Probably they both refer to the very same package?. A similar discrepancy appears for a lot of other packages, too. (For WLCSP it's a different matter.)

1 ACCEPTED SOLUTION

Accepted Solutions
FBL
ST Employee

Hello @Andreas Bolsch , 

You can refer to the datasheet DS13867 section 6.4 LQFP32 package information. This LQFP is a 32-pin, 7 x 7 mm low-profile quad flat package. Maybe, it seemed unclear in the CubeMX selector, but for now, it is already fixed. 

FBelaid_0-1691579206677.png

 

Thank you

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.


View solution in original post

1 REPLY 1
FBL
ST Employee

Hello @Andreas Bolsch , 

You can refer to the datasheet DS13867 section 6.4 LQFP32 package information. This LQFP is a 32-pin, 7 x 7 mm low-profile quad flat package. Maybe, it seemed unclear in the CubeMX selector, but for now, it is already fixed. 

FBelaid_0-1691579206677.png

 

Thank you

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.