2017-02-09 7:47 PM
I am a beginner in stm32 and I don't understand that how to download the code to the microcontroller.
I am also confused about JLink, SWD and st-link. What's the differences between them?
Where can I find these information on the datasheet?
Thank you!
#st-link #stm32Solved! Go to Solution.
2017-02-09 8:37 PM
SWD and JTAG are connectivity methods into the debug support contained within the chip.
The ST-LINK, J-LINK, U-LINK, etc are debugger pods that connect via the SWD/JTAG connection described above.
You'd want to review the Technical Reference Manuals, and associated data, related to the core provided by ARM, rather than the Data Sheets from ST
2017-02-09 7:57 PM
the nucleo and discovery boards are mbed-enabled. just drag the compiled .bin file to it and the st-link built in to the boards does the work.
2017-02-09 8:37 PM
SWD and JTAG are connectivity methods into the debug support contained within the chip.
The ST-LINK, J-LINK, U-LINK, etc are debugger pods that connect via the SWD/JTAG connection described above.
You'd want to review the Technical Reference Manuals, and associated data, related to the core provided by ARM, rather than the Data Sheets from ST
2017-02-10 1:26 AM
Thank you!
2017-02-10 1:27 AM
Thank you!