2017-07-02 01:59 AM
Thank you for your patronage.
I'm Japanese.
I connected ST-Link / V2 as shown below.
However, an error was displayed as shown in the figure below. I translate this into English.
�Fatal error : ST-Link: Failed to identify the target MCU. Please check the selected hardware and interface. Session aborted.''
2017-07-02 10:32 AM
Thank you for your advice. My target MCU supplied voltage is 3.3V. Your advice has been of great help.
2017-07-02 10:45 AM
Read again user manual chapter #4 of UM1075
Table 4. Than under table you could see.'1. The power supply from the application board is connected to the ST-LINK/V2 debugging and programming
board to ensure signal compatibility between both boards.' How do you think, what does it mean? ________________ Attachments : Screenshot_20170702-182712.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyZk&d=%2Fa%2F0X0000000b9k%2FPbXNtU6llVjk7GmT.k7WSDUF34YXjvfFmzGP8sq3a4U&asPdf=false2017-07-02 10:54 AM
Usually the 3.3v source on the nucleo is coming from the on board usb st link v2... Please make sure the target mcu has proper supply source. 1.5v is not an operating voltage.
2017-07-02 10:44 PM
Hi Inoue-san,
Try this.
ST-LINK VDD (Pin 19) -> Nulcleo 3V3 (SB2 OFF) or JP6(IDD)-VDD side (See UM1724)
STK-LINK VAPP (Pin 1,2) -> same as above.
NOTE: ST-LINK VDD is provided via 10 ohm.
VDD provides 3.3V from the ST-LINK side.
VAPP is monitor the target VDD.
2017-07-03 05:13 AM
Thank you for your reply. Your reply was helpful. But the problem is not solved.
I followed your advice as shown in the figure below.
But the same error appeared.
I found the following description in UM 1724.
So I changed the figure below.
But the same error appeared.
2017-07-03 05:18 AM
Sorry for late reply. It is difficult for me. I'll think about it.
2017-07-03 05:23 AM
Sorry for late reply.
I made sure the my target MCU supplied voltage is 3.3V.
2017-07-03 07:11 AM
Hi Inoue-san,
You should connect both VDD and VAPP to 3V3.
2017-07-03 07:48 PM
Thanks to everyone, I was able to solve this problem. Thank you very much.
2017-07-03 09:48 PM
Thanks a million!
External ST-Link does works!
I'm very happy