2022-02-28 5:45 AM
STMicroelectronics ST-LINK GDB server. Version 5.8.0
Copyright (c) 2020, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
LogFile Name : C:\WORK\NEW_PROJECTS_DEV_BOARD\prototype_1\prototype\CM4\Debug\st-link_gdbserver_log.txt
Logging Level : 31
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Enabled
SWD Debug : Enabled
Target connection mode: Attach
Reading ROM table for AP 3 @0xe00fffd0
Hardware watchpoint supported by the target
COM frequency = 4000 kHz
ST-LINK Firmware version : V2J37S7
Device ID: 0x450
PC: 0x1
ST-LINK device status: LOCKUP
Enter STM32_AppReset() function
NVIC_DFSR_REG = 0x00000009
NVIC_CFGFSR_REG = 0x00001100
ST-LINK detects target voltage = 2.94 V
Device in lock up state, possibly "read and debug" protected. Use monitor commands to remove the protection
ST-LINK device initialization OK
Waiting for debugger connection...
Waiting for connection on port 61234...
Accepted connection on port 61234...
Debugger connected
ST-LINK device status: HALT_MODE
Enter STM32_AppReset() function
NVIC_DFSR_REG = 0x00000008
NVIC_CFGFSR_REG = 0x00000000
------ Switching to STM32CubeProgrammer -----
-------------------------------------------------------------------
STM32CubeProgrammer v2.7.0-RC1
-------------------------------------------------------------------
Log output file: C:\Users\FMOHAM~1\AppData\Local\Temp\STM32CubeProgrammer_a20644.log
ST-Link Server is running on port : 7184
ST-LINK SN : 30FF6F065647373734141043
ST-LINK FW : V2J37S7
Board : --
Voltage : 2.93V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x450
Revision ID : Rev V
Device name : STM32H7xx
Flash size : 2 MBytes (default)
Device type : MCU
Device CPU : Cortex-M7/M4
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a20644.srec
File : ST-LINK_GDB_server_a20644.srec
Size : 39552 Bytes
Address : 0x08100000
Erasing memory corresponding to segment 0:
Erasing internal memory sector 8
Error: failed to erase memory
Error: failed to erase memory
Encountered Error when opening C:\ST\STM32CubeIDE_1.2.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_1.6.0.202101291314\tools\bin\STM32_Programmer_CLI.exe
------ Switching context -----
Error in STM32CubeProgrammer
Debugger connection lost.
Shutting down...
i did try to erase all the memory but it says its read protected and i checked in the options bites too there is no protection
2022-03-02 1:49 PM
can any one tell me where should i define i am using an internal clock
below, do i need to ENable HSE or LSE or CRS SYNC?