cancel
Showing results for 
Search instead for 
Did you mean: 

Hello, I have some problems programming a custom STM32F417 board.

SArzb.1
Associate

The Flash of the chip can't be programmed. Mostly the error is that writing the first byte failed. But sometimes it is able to write a few bytes. It even worked like 3 times. The behavior is consistent over STM32CubeProgrammer and ST-Link Utility, and JTAG and SWD.

There are some side effects:

  • STM32CubeProgrammer does not report the Flash size correctly. It reports 1M instead of 515K, ST-Link Utility reports correctly
  • Erasing the Flash does not always work
  • Sometimes the flash changes its content. Mostly switching between 2 or 3 values

Thank you for your help.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Do a through review of your design, perhaps with an ST FAE assigned to your account.

With good design, the JTAG/SWD should be quite robust.

Differences on a board level check for power and component issues.

For FLASH, the VCAP pins and capacitors being particularly important.

Don't float BOOT0

Have NRST connected to any debug headers.

Make sure VDDA and VDD are powered. Similarly digital/analogue grounds.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

3 REPLIES 3

Do a through review of your design, perhaps with an ST FAE assigned to your account.

With good design, the JTAG/SWD should be quite robust.

Differences on a board level check for power and component issues.

For FLASH, the VCAP pins and capacitors being particularly important.

Don't float BOOT0

Have NRST connected to any debug headers.

Make sure VDDA and VDD are powered. Similarly digital/analogue grounds.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
KnarfB
Super User

Lower the SWD clock frequency in the tools used.

hth

KnarfB

SArzb.1
Associate

@Community member​ thank you very much. VDDA was not connected.

Its working now.

@KnarfB​ Thank you for your help.