2019-01-08 4:10 AM
Hello,
after update Stm32 Utility to version 4.3.0 HardRst command stopped working.
In log I can see:
-HardRst is available only on ST-LINK/V2 with firmware V2J12S3 and later.
but I have connected ST-LINK V2 with V2.J32.S7 firmware.
2019-02-26 2:59 AM
I had the same problem.
I tried both upgrade and downgrade of ST-LINK/V2 FW but it did not help.
Installed Stm32 Utility v4.1.0 and now it works
There is a suspicious "new feature" in release notes for v4.2.0:
2020-07-22 1:26 AM
This is still not fixed in 4.5.0. Can we expect a fix soon?
2021-02-09 7:22 AM
Unfortunate this is still not fixed in 4.6.0. :(
I am currently use -RST combined with -C Hrst or -C UR. As far as I can see the main difference is that this command does a device connect first.