cancel
Showing results for 
Search instead for 
Did you mean: 

External Interrupt does not turn led on on HAL library

rowellsa
Associate

Hello, i am trying to run a simple code that toggles the built-in led when i press the built-in user button. I wanted to do this manually using HAL library functions, but for some reason i do not seem to get it right somewhere. The code generated using CubeMX software works, but when i try to code it on my own, i cannot turn the led on. This is the code, and it already is very similar to the code that mx generated. Is there a library or a function that i'm missing?

 

 

#include "stm32g4xx.h" #include "stm32g4xx_hal.h" int main(){ GPIO_InitTypeDef GPIO_InitStruct = {0}; HAL_Init(); __HAL_RCC_GPIOC_CLK_ENABLE(); __HAL_RCC_GPIOA_CLK_ENABLE(); GPIO_InitStruct.Pin = GPIO_PIN_12 | GPIO_PIN_13; GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING; GPIO_InitStruct.Pull = GPIO_PULLDOWN; HAL_GPIO_Init(GPIOC, &GPIO_InitStruct); GPIO_InitStruct.Pin = GPIO_PIN_5; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, GPIO_PIN_RESET); HAL_NVIC_EnableIRQ(EXTI15_10_IRQn); while(1){ void EXTI15_10_IRQHandler(void) { HAL_GPIO_EXTI_IRQHandler(GPIO_PIN_12); HAL_GPIO_EXTI_IRQHandler(GPIO_PIN_13); } void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin) { if(GPIO_Pin == GPIO_PIN_13) HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, SET); else if(GPIO_Pin == GPIO_PIN_12) HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, RESET); } } }
View more

 

 

3 REPLIES 3
Karl Yamashita
Principal

Why do you have EXTI15_10_IRQHandler inside the while loop? 

while(1){ void EXTI15_10_IRQHandler(void) { HAL_GPIO_EXTI_IRQHandler(GPIO_PIN_12); HAL_GPIO_EXTI_IRQHandler(GPIO_PIN_13); }

That is already in stm32xxxx_it.c file.

 

Did you enable the NVIC for that GPIO?

KarlYamashita_0-1719605466499.png

 

 

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.
CAN Jammer an open source CAN bus hacking tool
CANableV3 Open Source

Karl Yamashita
Principal

In your HAL_GPIO_EXTI_Callback you have no debounce routine. See this YouTube video to learn how to debounce a button using interrupt. https://www.youtube.com/watch?v=o0qhmXR5LD0

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.
CAN Jammer an open source CAN bus hacking tool
CANableV3 Open Source

Pavel A.
Super User

 a simple code that toggles the built-in led when i press the built-in user button.

Nothing is too simple for a beginner. So let's look at your code again.

* The code probably does not compile as is because there are nested functions? You cannot run the program unless it compiles without errors.

* Why two interrupts on pins 12 and 13? You wrote about one "built-in user button". Is it a Nucleo board? What is another interrupt for?