Associate II
Apr 12, 2024 3:57 PM UTC
Solved
Error: Mass erase operation failed. Please verify flash protection
- 3 replies
- 3917 views
Currently running into an issue with a custom PCB with a STM32H750 MCU on it. We use an SWD connection to connect to the debugging port. When I go to fully erase the external memory, I receive an error message that is "Error: Mass erase operation failed. Please verify flash protection". If I try and program the device using my binary file, it says the core is locked up. The other 9 boards program fine. Is this a hardware issue more than likely or am I missing something?