cancel
Showing results for 
Search instead for 
Did you mean: 

EDT Graphich Display with STM32F7 MCU

mids400
Associate III

Hi guys,

I'm working on a Projekt, that it should be STM32F7 interfaced with a EDT-Display but without using the Operating System or TouchGFX.

The Developer had designed the Board in a way, that nobody can use it directly without FreeRTOS or TouchGFX.

I've tried to using BSP_Library but not worked. It were designed in order to work only with the internal BootLoader.

The Board which i used shown in Attachement als a Picture and its Model is : ETEMB043013XDHAL

Anybody here have an idea about that?

1 REPLY 1
FBL
ST Employee

Hi @mids400 

Could you please be more specific and reformulate the issue? Maybe, we can help you! 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.