cancel
Showing results for 
Search instead for 
Did you mean: 

Cortex M4 draining a lot of current.

Andres P.
Associate
Posted on December 24, 2016 at 02:00

I'm doing a motor controller project, where I was using  STM32F446RET6 to learn how to work with an ARM processor. I designed the board myself.

Without the microcontroller soldered the 3.3V LDO was working fine and the power led was on (current consumption < 10 mA). When I soldered on the microcontroller, the capacitors and the oscillator, the microcontroller starts draining current. I have put the current limit on the power supply I used up to 150 mA max and the microcontroller drains all of it, while the voltage drops to around 2.9 V after the LDO (it should be 3.3V but because of the current limiter setting on the power supply it went lower).

According to the data sheet

http://www.st.com/content/ccc/resource/technical/document/datasheet/65/cb/75/50/53/d6/48/24/DM00141306.pdf/files/DM00141306.pdf/jcr:content/translations/en.DM00141306.pdf

on pages 83-85, it shouldn't use more than 100 mA. I measured the resistance between all the MCU pins and ground and there didn't seem to be an anomaly, also checked for bridges between the pins under a microscope. Using an oscilloscope I measured that NRST was high and the input voltage wasn't oscillating. I couldn't detect a clock on the OSC pins, it seemed more like a 10 mV random noise

Also when I compared my schematic, attached below, to the hardware development guide

http://www.st.com/content/ccc/resource/technical/document/application_note/76/f9/c8/10/8a/33/4b/f0/DM00115714.pdf/files/DM00115714.pdf/jcr:content/translations/en.DM00115714.pdf

, it seems that my design should work.

So I was wondering if maybe someone can point out that there is something wrong/missing on my scheme or can confirm that maybe the 150 mA limit is too low and I should just try increasing the limit? Or maybe you can hint me as to what might be the problem. I was afraid of increasing the current limit because it seems a lot already and I thought there must be a problem and I might fry something.

In the schematic you can ignore the motor driver and the USB-UART chip on the second page, as these haven't been soldered. I have only soldered the LDO, the power LED, the three buttons, the microcontroller with its oscillator and the relevant capacitors/resistors. I have also soldered the USB socket and the USB ESD protection.

As a next step I thought about desoldering the oscillator and trying to run it with only the internal oscillator. Then I thought about desoldering the USB ESD protection, maybe it is interfering. But other than that, if anyone can't point out an error in my schematic, I should try to solder a new MCU because maybe I somehow fried it while soldering (but that's not likely I guess)?

#pcb-design #high-current #schematic
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Posted on December 24, 2016 at 03:30

Don't connect VCAP_1 to VCC, the VCAP pin is the 1.25V output from the internal regulator.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

1 REPLY 1
Posted on December 24, 2016 at 03:30

Don't connect VCAP_1 to VCC, the VCAP pin is the 1.25V output from the internal regulator.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..