cancel
Showing results for 
Search instead for 
Did you mean: 

Can you ground both VDD50USB and VDD33USB if you are not using USB features?

shffhsdfhse
Associate III

The datasheet is a bit light on details about what to do with these pins if you are not using USB at all. Can I ground both of them, or does there need to be a supply voltage on VDD33USB?

One of the notes on the Absolute Maximum Ratings section in the datasheet says "All main power (VDD, VDDA, VDD33USB, VDDSMPS, VBAT) and ground (VSS, VSSA) pins must always be

connected to the external power supply, in the permitted range," but I don't know if this means that ground is a valid "external power supply."

For example, in other parts of the datasheet it says that VBAT must be connected to VDD even if a battery is unused. However, it also says VDDSMPS should be connected to GND if unused. So I am unsure about the meaning.

1 ACCEPTED SOLUTION

Accepted Solutions
FBL
ST Employee

Hi @shffhsdfhse 

 

Check FAQ: Configuring the VDD50USB and VDD33USB pins on... - STMicroelectronics Community

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.


View solution in original post

1 REPLY 1
FBL
ST Employee

Hi @shffhsdfhse 

 

Check FAQ: Configuring the VDD50USB and VDD33USB pins on... - STMicroelectronics Community

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.