2020-04-22 6:18 AM
I have followed Video "STM32CubeIDE basics - 03 GPIO HAL lab" as closely as possible for my hardware as closely as possible and get the following results in the console:
STMicroelectronics ST-LINK GDB server. Version 5.5.0
Copyright (c) 2019, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
-------------------------------------------------------------------
STM32CubeProgrammer v2.4.0
-------------------------------------------------------------------
ST-LINK SN : 9877000132124647524B4E00
ST-LINK FW : V2J36S7
Voltage : 3.19V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x410
Device name : STM32F101/F102/F103 Medium-density
Flash size : 128 KBytes
Device type : MCU
Device CPU : Cortex-M3
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a08984.srec
File : ST-LINK_GDB_server_a08984.srec
Size : 7600 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 7]
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:01.741
Verifying ...
Download verified successfully
Debugger connection lost.
Shutting down...
The ST-Link is a third party device . I have tried two different samples of the ST-Link from different suppliers. I have also tried two Blue-Pill devices from this batch.
I have also tried a Blue Pill device from another batch which reports:
Error in initializing ST-LINK device.
Reason: ST-LINK: Could not verify ST device! Abort connection.
and I suspect a faulty or fake chip.
Any help would be much appreciated so I can get on with development instead of Tool Chain Tinkering!
2020-04-22 8:55 AM
Found it. Stupid really. If there isn't a break point in the code, the debugger disconnects and the program keeps on running. J
Just add a break-point to the code.