cancel
Showing results for 
Search instead for 
Did you mean: 

ARM Debug probe with power to target capability

Gaston
Senior

I have been using PE micro Multilink FX for several years, but its Linux support is terrible. Is there a ST (or another) alternative with this functionality compatible with stm32CubeIDE? I just need to supply power (up to 100 mA at 3.3V) to my board for debugging. I don't need high tracing performance or anything like that.

Thanks in advance,
Gaston

10 REPLIES 10

The right adapter for this purpose would be this:
https://www.segger.com/products/debug-probes/j-link/accessories/adapters/target-supply-adapter/

"The Target Supply Adapter provides an adjustable supply voltage to the target board. It has a standard 20-pin 0.1" socket towards the J-Link debug probe or Flasher in-circuit programmer, and a standard 20-pin 0.1" header on the target side and can directly be inserted between the J-Link or Flasher and the debug cable maintaining a 1:1 connection of all debug signals. The supply voltage to the target is provided through pin 19 of the debug cable."