2023-05-23 7:58 AM
Hi everbody. I've developed a project for STM32H7A3IIK6 [BGA package] and i've mounted the bypass capacitor on the same side of the MCU [not on the opposite side as suggested by STM Application Note] because of problems related to my production process. Now i'd like to write an application to stress my MCU in climatic chamber to understand if, in this configuration, i could have problems like HardFault or similar. Is there in CubeMX or in some github STM repository, for this MCU [or similar], any kind of benchmark/application to stress the MCU? Could you suggest me what to implement to stress the MCU?
2023-05-23 8:01 AM
Hello @Community member ,
I suggest you this link : STM32CubeH7/Projects/NUCLEO-H7A3ZI-Q at master · STMicroelectronics/STM32CubeH7 · GitHub
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-05-29 3:20 AM
Thank you so much @KHALSI_Foued . I'm looking for a benchmark to test the power of a STM32H7A3IIK6. A good test for this purpose could be a dhrystone or a whetstone example test but i've not found anything already implemented.Do you know where i could find something like this?
2023-05-29 3:45 AM
You can find some results about the coreMark in the DS: Datasheet - STM32H7A3xI/G - 32-bit Arm® Cortex®-M7 280 MHz MCUs, up to 2-Mbyte Flash memory, 1.4-Mbyte RAM, 46 com. and analog interfaces, SMPS ( Table 37. Typical consumption in Run mode and corresponding performance versus code position )
Check also product presentation : microcontrollers_stm32h7a3-b3_line_product-overview.pdf
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-05-29 4:22 AM
Ok @KHALSI_Foued . But what i need is a benchmark example, like the one used by ST to build the report of Table37 of the DS, because i have to evaluate, in my own application, if i can mount the bypass capacitors on the same side of the MCU or if i need to mount them on the opposite side [it's a BGA package]. My problem is that, for my production line, it's better to mount the capacitors on the same side of the MCU.