cancel
Showing results for 
Search instead for 
Did you mean: 

ADCs - QUEUE

Marc3
Associate

Hello, 

 

I have a NUCLEO U545 - REQ and i have a Queue in which i read the incoming values from 4 potientiometers from my ADC4 and send them directly into the DMA. 

 

The problem is that i also have the ADC1 connected to some potentiometers and im not able to put two ADC reading nodes into the same Queue. If i look at the live expressions i the readings of the ADC4 get stuck into the "first iteration" while the readings of the ADC1 do not initialize and therefore the Queue gets in this ADC1 reading node. I have not found any problem related to Queues and Nodes in the forums but i have found some videos about it and theres no example about two adc reading nodes inside of the same queue. Therefore i suppose i have to create a different queue but how do queues interact with each other? 

 

Does someone know how do Queues interact with each other or is there any way of creating two ADC reading nodes in the same Queue? 

 

Thank you,

 

Marc

0 REPLIES 0