cancel
Showing results for 
Search instead for 
Did you mean: 

5V Tolerant (FT) Pins with Internal Pull-down Resistor on STM32H753ZI

aditya3
Visitor

Hi,

I am using a STM32H753Zl MCU and have configured an FT pin (PCO) for 5V digital inputs. However, since the pin is floating I have enabled the internal pull-down resister via CubelDE. While testing it worked fine, but is there any
damage this could cause to the board in the long run?

Thanks

1 REPLY 1
Peter BENSCH
ST Employee

If you look at the data sheet, you will find two statements:

Section 7.2, table 118:

  • VIN, Input voltage on FT_xxx pins = max Min(VDD, VDDA, VDD33USB, VBAT) +4.0V
  • Footnote (4): To sustain a voltage higher than 4V the internal pull-up/pull-down resistors must be disabled.

This means that the pull-down can withstand 5V when VDD is applied - the emphasis here is on ‘applied’. If VDD is switched off and therefore 0V, you exceed the above condition by 1V.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.