2024-04-23 05:17 PM
2024-04-23 06:47 PM
Like you're driving signals into the wrong pins, there's a short, or the grounds aren't properly/effectively bonded.
2024-04-23 07:26 PM
能给出更详细的解释吗?
2024-04-23 08:15 PM
>>Can you give a more detailed explanation?
Not really, you've not really presented your entire circuit or wiring.
The inter-modulation you're showing is likely due to driver pins being shorted together, or having some conductive path through resistors. Perhaps pull-up / pull-down resistors to a floating node, rather than being one of the rails.
Or you have ineffectual grounding in the system.
Hard to tell from here, you're going to have to debug your own circuits, and think about possible causes.
I don't see you configuring multiple UARTs on the STM32 side will do this.
Check the pin configurations, especially those presenting the signals shown.
2024-04-23 11:07 PM
找到原因了,是tx和rx原理图出反了😂