2022-06-29 6:57 PM
I am using ST25DV. Access from RF must be restricted.
I'm trying to use RFSwitchOff / RFSwitchOn for this purpose, but NACK is returned.
Before using these, I changed the I2C_CFG setting in the System register to 0x3A (I2C_DEVICE_CODE: 1010, I2C_E0: 1, I2C_RF_SWITCHOFF_EN, 1).
I got the value of I2C_CFG of System register and confirmed that it is 0x3A.
And I use the following address.
Start condition + RF Switch Off or On->NACK
Please give me some advice to solve this problem
Solved! Go to Solution.
2022-07-05 1:57 AM
Hello Haru,
May be a stupid idea, but this feature is available only in the ST25DVxxKC (C) version, not in the ST25DVxxK version. So, may be you are using a ST25DVxxK version ?
Can you please provide the UID or the IC_REF of your ST25DV ? (to check which version you are using)
Best regards.
2022-07-05 1:57 AM
Hello Haru,
May be a stupid idea, but this feature is available only in the ST25DVxxKC (C) version, not in the ST25DVxxK version. So, may be you are using a ST25DVxxK version ?
Can you please provide the UID or the IC_REF of your ST25DV ? (to check which version you are using)
Best regards.